Encyclopedia search

Reset search
Showing 51 to 60 of 438 results
CFC (Chlorofluorocarbon)
CFC and HCFC refrigerants are detrimental to the breakdown of the ozone layer and the greenhouse effect. CFC is an abbreviation of chlorofluorocarbon; HCFC is an abbreviation of Hydrochlorofluorocarbon. They describe the molecules’ atom content.
Channel impeller
A channel impeller works directly on the pumped liquid with the liquid passing through the impeller itself. A channel impeller can be described as a closed, semi-open or open impeller.
Channel impeller
A channel impeller works directly on the pumped liquid with the liquid passing through the impeller itself. A channel impeller can be described as a closed, semi-open or open impeller.
Charge exchanger
A charge exchanger combines the advantages of both a traditional domestic hot water exchanger and a hot-water vessel
Charge exchanger
A charge exchanger combines the advantages of both a traditional domestic hot water exchanger and a hot-water vessel
Chilled beams
Passive and active chilled beams are used for cooling building air. Passive chilled beams cool the inside air without the noise and expense of ductwork and air handler units. Active chilled beams generally have much higher sensible cooling capacities than passive chilled beams.
Chilled room
A chilled room is a refrigerated area for cold storage of perishable items, especially food, to preserve them. In a chilled room the temperature is typically between 0 - 5°C.
Chiller
A chiller is a component that is used to cool water. The cooled water is pumped from the chiller to a water/air or water/water heat exchanger, where it can be used to cool air or water respectively.
Chlorination
Chlorination is probably the most common method of treating microorganisms in water. This method is mainly used by water utility companies in order to kill microorganisms in water right from the water production site up to the consumers water tap.
Chlorine dioxide
Water disinfection with chlorine dioxide is a very efficient and gentle way of fighting legionella bacteria and all kinds of micro organisms in water such as viruses, parasites and fungus spores.